Other Parts Discussed in Thread: UCC3803, LM5155
Dear Support Team,
I'm currently designing a circuit that requires a power supply with the following requirements:
- Input from a single 12V battery
- Two outputs around +24V and -24V (the exact value and symmetry is not so important)
- Output power : at least 35 Watts, shared between the two outputs
- No insulation required between input and outputs
- No BGA or QFN packages. If possible, avoid VSSOP.
Now, there are a lot of boost controllers available like the LM3478, which is simple enough for me.
I came across an application notes for making a dual output supply out of a boost controller with a UCC3803, using a charge pump made of discrede components and capacitors:
https://www.ti.com/lit/ds/symlink/ucc3803.pdf?ts=1699154399763
Is it possible to apply the same principle to the LM3478 and stay within design requirements?
Kind Regards,