Hello Experts, TPS7A8301A, TPS7A8300A is 2A Iout LDO. Can you suggest a similar LDO with 3A or 4A Iout where the voltage can be adjusted in steps using pins (25mV, 50mV, 100mV, 200mV......). I plan to drive these voltage configuration pins (1 or 0) using FPGA IOs to sweep the LDO output voltage.
thanks, Abhijit