Hi,
Currently, due to Intel Apollo Lake stepping up to F-1, we observed that after the replacement, the frequency can only reach 2.2 GHz or 2.1 GHz, instead of the 2.4 GHz in B-1.
The multiplier seems to be stuck at 21-22 and cannot reach 24. When measuring, we noticed that both sets of VCORE voltage are slightly higher than in B-1. There don't appear to be significant differences in other BUCK components.
We are currently using TPS650942 & TPS650947, and it seems that both are facing this issue.
What could be the possible reason for this? Do we need to modify any settings in the PMIC.
By checking through PMIC_I2C, we found that the F1 CPU writes a voltage value higher than the previous B1 version during the boot BIOS stage.
After entering the boost state to run at the highest frequency, the original B1 CPU writes a stable voltage value directly.
However, the F1 CPU continues to cycle rapidly, switching between two levels with a 0.01V difference.
There have been no specification changes on Intel's side, and we suspect it may be due to IMON differences.
However, TPS650942/650947 do not have an IMON pin that can be configured.
What could be the reason for the PMIC continuously sensing and adjusting the voltage? The peripheral circuits are all the same.
Thanks!
Jeff