Part Number: UCC27528-Q1
Other Parts Discussed in Thread: UCC27528, UCC27301A-Q1, UCC27301A, UCC27311A-Q1, UCC27284
Hello Experts ,
In our application one of the constraint is Quiescent current drawn by gate driver should be less than 100uA (less than 50uA) is preferable . Gate driver will be operated by DC ON or OFF signal (not a switching application )
UCC27528 datasheet has below Iqq , Can we consider this as steady state current when gate output is not switching ? (Either Gate output will be high or Low)

As per dynamic specifications , Gate driver current will be more than 1mA while gate output is switching .
Please clarify on this.
Also suggest if any Low IQ low side gate driver is available ?
thanks
Regards
Vasu