Hello,
We already exchanged on one of our design on the linked post with yihe.
We are encountering a very strange issue with that same design, on the equation of the TMS_GPIO21 output pin (HWRST_Ni on the schematic sent through our FAE Franziskus Hillreiner).
The configuration of the GPIO is the following :
All signals except the FB_LBK_HWRST_N are active high inputs.
We have checked on the board with an oscilloscope and all the inputs except the FB_LBK_HWRST_N are low. However, we would have expected HWRST_Ni to be high at board level and it is low.
We confirmed these levels with the Monitor task in Fusion Digital Power Designer.
This does not make sense.
We encounter this behavior after some tests which leads to the FB_LBK_HWRST_N toggling (due to UV generated on the MON inputs) between high and low with DIS_RESET_GEN low to ensure the HWRST_Ni is not set during these tests, when we set DIS_RESET_GEN back to high state after FB_LBK_HWRST_N being high during at least 40ms.
We do not encounter this behavior each time, we couldn't figure out a pattern of occurence, and it happens on two UCD9090-Q1 of our board.
Anything you see we could be doing wrong ?
Best regards,
Clément