This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61099: Low efficiency problem

Part Number: TPS61099
Other Parts Discussed in Thread: TPS61299

Hi TI Teams,

One of our customer reported that the efficiency is only 74%~76% with the real load like MCU,small fan and laser (the laser is switched on at 0.5s intervals, and the other loads run continuously). However, the efficiency is above 90% when tested with dummy loads. They also tried adding a 22uH Π filter circuit to the output, which would increase efficiency by 3%, but it didn't meet the requirements. The efficiency difference is only 3% with different inductors.

The schematic and layout is as below:

Do you have any good suggestion for this problem?

Thanks,

Kind Regards