This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR36520: UVLO settings

Part Number: LMR36520

Hi team,

Having a few questions regarding the UVLO settings of the device.

1. There are VEN-H and VEN-HYS in the following calculation on the datasheet, but I didn't find these 2 parameters on the EC chart.

Are these the same as the following values?

2. Is there a range limit for Von with UVLO? My customer wants to set the device on upon 20V input voltage.

Regards,