This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25180: EN_PUSH register doesn't seem to work as described.

Part Number: BQ25180


Hello - 

In the datasheet, it says that the EN_PUSH being set to '1' would only enable the button detection functionality when on battery only.

What I observed is actually different.

When set to '0', it only enables the button detection when there is VIN present. If only the battery is there, it doesn't seem to work.

When set to '1', it detects the button presses regardless of whether VIN is present or not. 

Could you check whether the description in the datasheet is correct?

Thanks a lot!

Olivier