Other Parts Discussed in Thread: , TPS7A39, , LM317
I am trying to add current limiting to the previously submitted design by adding LM317 and LM337 regulators in current-limiting mode. Both simulate nicely standalone but don't deliver usable results in combination with the TPS7A39. Ideally I would like to place them inside the output feedback loops of theTPS7A39 for better voltage regulation, but neither this approach nor placing them before the TPS7A39 delivers any usable simulation results at all. Depending on the simulation parameters, the simulation fails to converge, never finishes or shows kilovolt spikes at the negative input of the TPS7A39. The only configuration that comes close to delivering believable results is putting the current regulators after the (closed loop) TPS7A39 voltage regulator. However, the LM337 shows no output at all in this configuration, even though it shows a normal output when fed by an ordinary rectifier / capacitor circuit instead of the negative output of the TPS7A39. I am using the LM337-N from the included PSPICE for TI library, although the finished design should use the LM337L. The attached project archive should include 3 different designs, but I am uncertain about the relationship between projects and designs. I have also attached a screenshot of the simulation results showing a flat line for the output of the LM337 (purple) in contrast to the expected output delivered by the LM317 (yellow).

P.S. Here is a screenshot of the schematic as insurance: