Part Number: TPS543320
Hi TI.
We are using a voltage divider from Vin to GND to control the Enable pin, and has calculated values to stop at 9.25V (Nom) and start at 10.1V (nom).
The start value is quite precise but the device doesn't stop until Vin is at 6.9V.
In the datasheet equation 1 and 2 calculates the resistors to be used. We did not use this, be relied on the Ven values. This has given us R_top=200k and R_bottom =27k
I wanted to recalculate using equation 1 and 2, but the equations mentions two costant current sources Ip and Ih, but the values for them are not given anywhere in the schematic.
Can you help with this?
BR Henrik Buhl