I need to calculate the junction temperature of the TLV76012 component in my application. I have measured the temperature on package top with an IR camera, and it is 84 ºC at an ambient temperature of 20 ºC. The component dissipates 0.8 W and is mounted on a 0.7 mm thick, 2-layer board. The board is also mounted on a large heat sink. I think the Jedec thermal resistance provided in the datasheet of 2.9 ºC/W may not correspond well to my application. Therefore, I would perform the calculation using the Rjc of 92.9 ºC/W.
So the calculation would be: Tj= 84ºC + 0.8 W*92.9= 158.3 ºC, so it might not work correctly.
However, using the Jedec thermal resistance, the calculation would be: Tj= 84ºC + 0.8 W*2.9= 86.3 ºC, so I could use the component.
Which thermal resistance value should I use?
Comparing with the Jedec, isn't the value of 92.9 ºC/W too high? Is that value correct, or is it an error in the datasheet?