Part Number: BQ34Z100-G1
Other Parts Discussed in Thread: BQ76942, , TIDA-010030, BQ34Z100, BQ34Z110, BQ34110
I have some questions regarding the BQ34Z100-G1 device in combination with a BQ76942 monitor:
I have a setup where i want to combine the BQ76942 Monitor with BQ34Z100-g1 as top of stack fuel gauge. Everything should work in stand alone(Monitor programmed via OTP) and i want just to read from the battery pack. The questions are about how I can reduce power consumption in shutdown mode and whether this is also permissible with the fuel gauge. The monitor can be placed in a shutdown mode where it consumes approximately 1µA of current. Unfortunately, the lowest current consumption of the fuel gauge is approx. 30µA in fullsleep.
Question 1:
Is it OK to disable the fuel gauge when the monitor is in shutdown mode? I think I read once that the fuel gauge should always be connected to the battery because it takes measurements from time to time. In the reference design TIDA-010030, the fuel gauge is deactivated and the power supply is switched off when the monitor is in shutdown or shipping mode. Is this a good and approved approach? Or should the fuel gauge always be connected? I think that would drain a smaller buttery pack over time
Question 2:
Unfortunately, the data sheet does not contain much information about the CE pin of the fuel gauge. Its also hard to test because the EVM does not expose that pin separately. Could this pin be used (if question one allows) to deactivate the fuel gauge and thus reduce power consumption when the monitor is in a shutdown state? How high is the quiescent current of the pin and are there voltage levels that result in a low or high state available? I could not find it in the datasheet? (I Think about to drive this pin via a GPIO from the monitor because the data sheet mentions a possible GPIO usage: Can be configured for an active-high output to be driven from the REG18 LDO)
Thank you for your help in advance