This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS1641: output current limit MIN/MAX @ 250mA

Part Number: TPS1641
Other Parts Discussed in Thread: TPS2660

Hi TI support,

I found the TPS1641 and I realy like it.

For my design I need a more precise answer than the 3 lines in table 7.5 with Rlim=332kOhm, 10kOhm and 5,49 kOhm. I see the accuracy is not the same with different resistors, but is it perhaps like the figure 24 in TPS2660 datasheet?

I will use Rlim = 40 kOhm to get Ilim = 250mA. But what are the MIN and MAX values?

Thank you very much!

Best regards

Markus