This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
We are currently designing converter circuit using LMZ14201 IC with Vin=24V, Vout=15V with Max load <1A (IC supports up to 1A max) with startup time being 0.5ms considering Css=4.7nF
To start with we tried with the simulation package that is provided in the TI website https://www.ti.com/product/LMZ14201H#design-development.
However, with RFBT = 34K, RBBB = 1.91K to generate Vout = 15V considering Cout = 2x 10uF, we are reading Vout = 14.73V to 14.89V during line regulation (18V to 24V) and startup time being 2.2ms
Also, tried the same with the EVL board but Vout measurement is 16V during low load (0.1A to 0.3A) and Vout = ~15.3V at max load (0.7A - 1A)
Q1: Does this IC capable to convert output voltage close to Vin (24V to 15V in the above case).
Attaching the simulation circuit and results for reference.
Hi Vinod,
Thank you for sharing your scope shots and schematic. According to the datasheet, the LMZ14201 is set to work with input voltages ranging from 6 to 42 V and output voltages ranging from 0.6 to 6 V. TI does not guarantee nor recommend operation with VOUT of 15 V. I have included the datasheet link and a snapshot for your convenience.
Thank you,
Joshua Austria