Other Parts Discussed in Thread: BQ25185
Hello,
I am using BQ25050 in my new design with #CNTRL pin kept floating ( I am okay to use default current of 285mA ) and #CHG pin connected to LEDs for indicate charge status.
The schematic image is attached for reference.
Once connected 5V USB VBUS voltage, it is noticed that fast charging is happening with 280mA but termination is not all happening even Ichg current is less than 7.5% of 285mA.
I measured with a ammeter and noted that after a long period of time ( appx 9-10 hours) ICHG =appx 1mA but still #CHG pin are LOW .
The LEDs connected to #CHG pin through P-MOS are still glowing with ICHG =1mA. It is understood that , termination is never happens.
Could you please check the circuit and suggest the solution.
Regards
PSG