Other Parts Discussed in Thread: TPS629210, TPS63700
Hi support team,
Is it possible to use TPS6040x in the following ways?
I want to input negative voltage and output negative voltage.
VIN = -5V
VOUT = -10V
Regards,
Dice-K
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Dice,
In that case, you just need 1*TPS6040x. The first stage should give you -10V. In any case, I suggest to try this config using our EVM and test it thoroughly before actual implementation.
May be you could also consider TPS63700 as an alternative.
Regards,
Febin
Hi Febin,
Thank you for your support.
I have understood that there is no need for double use as shown in Figure 9-8, and that it can be realized in theory with a single use as shown in the figure below.
Best regards,
Dice-K