HI engineers:
About the TPS92692 dimming Contrast Ratio, How do I calculate dimming contrast 15:1 , or can you Provide the formula?
Thank you.
Johnsin Tao
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI engineers:
About the TPS92692 dimming Contrast Ratio, How do I calculate dimming contrast 15:1 , or can you Provide the formula?
Thank you.
Johnsin Tao
Johnsin,
I assume you are asking about the analog dimming ratio of 15:1 from IADJ. It's just the ratio of the highest command DC current from IADJ to the lowest current from IADJ command. For example, if the max current command with IADJ of 2.25V is 1A then the minimum current that you will be able to 1/15 = 66.67A.
Thanks Tuan