This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM74670-Q1: Cannot get device to switch FET

Part Number: LM74670-Q1
Other Parts Discussed in Thread: LM74610-DQEVM

We are developing a bridge rectifier with ideal diodes. Max current is low (<100mA),  AC input voltage 10Vpp.

We were originally going to use the LM74610 device because the datasheet showed it could cope with a 60Hz AC input (see pic below). This is obviously a mistake in the datasheet because we learnt that this device is too slow for our application which is around the 200Hz mark. We were able to get the device switching correctly at 1Hz max only.

We then replaced one of the LM74610 devices on the LM74610-DQEVM PCB with a LM74670 device, but have not been able to produce any rectification ...we just see the AC input voltage at the output i.e. no rectification at all. (Note, we are not powering the 2nd LM74610 device on the PCB at all). We tried several values for VCAP i.e. 0.47uF to 2.2uF with little effect. 

Can you please provide some suggestions on what to do?