Hi, TI expert.
A customer is reviewing the TPS23754 and has a question in the Application note (High Efficiency Class 4 PoE Powered Device).
Looking at the schematic of the demo board shown in the application note (High Efficiency Class 4 PoE Powered Device), Capacitor, ceramic, 1000 pF, 2 kV, X7R, 10%, 1808 spec was applied to C5 and C4.
Is there a reason to use 2KV for internal voltage?
Will there be a problem if I apply a value lower than 2KV?
Are there any problems if the (Bob smith termination) value of C5 is changed?
Please check. Thank you.