This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR38020-Q1: LMR38020

Part Number: LMR38020-Q1

Hi,

I have using LMR38020-Q1 for Step down the voltage.  im facing the issue in current consume without load 10mA.

kindly suggest to achieve <2mA. 

Below mentioned is configuration.

Inpunt voltage: 6 to 70V

Nominal: 12V or 24

Output: 4.7V

SW frquency: 500Khz

Iout:2A max

Circuit: