This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS568230: Fsw range

Part Number: TPS568230

Hi Team,

Customer requested Fsw range SPEC. DS only provides TYP value. Could you kindly advise MIN and MAX value for Fsw?

TPS568230:

Thanks and best regards,

Terry

  • Hi Terry,

    Our US team will reply you next Monday.

  • Hi Terry,

    TPS568230 us a DCAP3 device and it does not have any internal oscillator to set switching frequency. So the switching frequency min/max is not directly specified since the switching frequency is dependency to Vin/Vout/Iout/FCCM /OOA/ECO mode. You can get an idea of its variation by looking at figure 20-28 in the datasheet. 

    If this resolved your issue, please click "This resolved my issue". Thanks,

    Nancy

  • Hi Nancy,

    Sorry for the unclear description.

    Customer set the device at FCCM mode, Fsw 600KHz by external resistor divider(110K/51K) at mode PIN.

    They would like to know the reference Fsw distribution range for this setting.

    We know that DCAP3 devices Fsw will change due to many factors. Thus, a distribution range only for reference is OK. No need for a guarantee value. 

    Could you please advise?

    Regards,

    Terry

  • Hi Terry,

    Please refer to Figure 26 in the datasheet for 600kHz range as below. We don't have distribution data available.

    Hope this helps,

    Thanks,

    Nancy