This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP5860: LP5860 support need

Part Number: LP5860


Hi team,

There is a question of LP5860 from GREE need you support. The max average current of each LED dot is less than 5mA when the Iout_max = 50mA and the scan number is 11, is that correct? 

If that is correct, that means the average current of each LED dot is too small. So if there is other device which can load bigger current in each LED dot?

Thank you very much.

Best regards,

Ryker