Part Number: LM5012-Q1
Other Parts Discussed in Thread: LM5012
Hi Team,
We have developed a LM5012 based buck convertor.
Designed parameters:
Input Voltage 15 to 60V
Output Voltage 5
Output Current 2.5A
1. When no load is connected, output is stable between 5.01 to 5.1V
2. When load (0.5A, 10ohm, 5W wired wound resistor) is connected across output, the load output voltage is fluctuating between 3.8V - 2.8V for 15V - 60V input.
Reference Circuit

Kindly help us with the solution.