Hi Expert
I tried to understand the CFF calulate and I have some question need your help
the equation shows below in datasheet : my Cout : 66uF, VREF=1V, Vout=3.3V, RFBT=100K , chip freq=2MHz , Loading current from 150mA to 3A

My CFF result : less than 31.97pF
and Using Webench to check my PM/GM/CROSSOVER FREQ
So, I sweep the CFF value on websim shows below
CFF=30pF GM::19.36 PM: 90.75 Crossover Freq.:44.6k
CFF=33pF GM: 18.8 PM: 91.75 Crossover Freq.:41.93k
CFF=56pF GM: 16.21 PM:84.16 Crossover Freq.:71.21k
CFF=68pF GM: 15.46 PM:76.93 Crossover Freq.: 80.02k
CFF=100pF GM:14.29 PM:64.66 Crossover Freq.:90.81k
I means, these CFF value seems no stability problem with oberserve from PM/GM/CrossFreq.
Question : Why the equeation setting like that? Something I misunderstand or ignore the from design?
Should I notice something in larger CFF value? or some operation condition?
Can expert help me out of this ?
(I know it will imporve transient reponse by increase crossover freq. that's our target, too.)
Reference doc attached, thanks!!
CFF_Evaluation and Performance Optimization of Fully Integrated DC-DC Converter.pdfslva289b_CFF Com.pdf