Hello,
I have two questions related to the LM61495-Q1:
- The maximum junction temperature stated as 150oC, but the thermal shutdown tripping threshold is 168oC Nom. can you please elaborate on that ?
- What's the efficiency of the device when the input voltage is too low to provide the desired output voltage (for example 9V input and 11V output setting) - Is there any additional current limitation when the device is operating in such mode ?
Thanks,
Yassine