This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27Z561EVM-011:how to write the golden files

Other Parts Discussed in Thread: BQ27Z561EVM-011, BQ27Z561

部品番号: BQ27Z561EVM-011

拝啓。

 BQ27z561EVM-011 を使用したゴールデン ファイルを作成しました。
 添付ファイルをご参照ください。

 環境ボードは 4 つあります。(BQ27z561EVM-011)

 ゴールデン ファイルを BQ27z561EVM-011 に書き込みました。
 1 つの環境ボードが正しかった。
 もう1つの環境ボードがエラーでした。
 エラーはコマンド「C: AA 3E 02 00 15 61 00 04」に対する「02 00 15 61 02 01」の応答でした。
 原因はBQ27z561のファームウェアバージョンの違いでしょうか?

 ゴールデン ファイルを作成した BQ27z561 のファームウェアのバージョンを教えてください。 
 また、「02 00 15 61 02 01」というエラーが表示されるBQ27z561のファームウェアのバージョンは何ですか 

 ファームウェアのバージョンの違いを無視してBQ27z561にデータフラッシュテーブルを書き込んでも大丈夫でしょうか?

よろしくお願いします、1561_0_04-bq27z561.gm.zip

  • こんにちは、

    アドレス構造が変更される可能性があるため、ファームウェアバージョンの違いを無視してbq27z561にデータフラッシュテーブルを書き込むことはお勧めしません。

    現在ボードに搭載されているファームウェアのバージョンを確認できるように、ゲージの.ggファイルを送信してください。

    Regards,

    Anthony Baldino

  • Dear Baldino san

     Thank you for your replay.

     I attach two .gg file.
    The 230831.gg.csv's BQ27Z561 was used to create the golden file.
     And, We tried writing the golden file to the 231201.gg.csv's BQ27Z561.
     Result is error.
      230831.gg.csv231201.gg.csv

    Best regards,

  • Hello,

    There is a difference between the firmware of these two devices:

    230831.gg firmware is version 0.04.

    231201.gg firmware is version 2.01.

    This could be why the golden image is not able to be programmed to the newer version.

    The most recent version of the firmware can be found in the bq27z561 product page under Software Development:

    https://www.ti.com/product/BQ27Z561#software-development 

    Regards,

    Anthony Baldino

  • Dear Baldino san

     Thank you for your reply.

     Please tell me if you know how to convert the golden file created with Ver 0.04 to a golden file for Ver 2.01.
     For example, conversion tool, etc.

    Best Regards,

  • Hello,

    Can you please tell me the process that you are trying to upload the .srec?

    Is the gauge you are trying to program in Unsealed Full Access/

    Regards,

    Anthony Baldino

  • Dear Baldino san

     Thank you for your reply.
     We have the .srec, the .bq.fs, the .df.fs and the .gm.fs. that we created by version 0.04 of BQ27Z561.
     We want to conversion those file into for version 2.01 of BQ27Z561.
    Can I conversion those file?

    Best Regards,

  • Hello,

    We believe that the issue could be coming from the gauge not being unsealed. The .srec created by the version 0.04 should be able to be programmed onto the version 2.01 since the .srec file contains the firmware of the gauge. Programming a file such as the .df.fs that only contains the configuration files could be an issue since it does not contain the firmware.

    Can you please tell me what security mode the version 2.01 gauge is in?

    Regards,

    Anthony Baldino

  • Dear Baldino san

     Thank you for your reply.
     We hoped to use .gm.fs file.
     We wanted to convert the .gm.fs to match the data flash table changed from Version 0.04 to Version 2.01.

    Best Regards,

  • Hello,

    We do not offer a conversion tool for the .gm.fs, however it is possible to extract the .gg file from the v0.04 gauge, update the firmware to the version 2.01, compare and input the data flash values, and then pull the .gm.fs to be used on the other gauges.

    Regards,

    Anthony Baldino