Hi TI Team,
1. Can you please clarify difference between TPS563207 and TPS563207S ?
2. Is there any limitation on Max output capacitance?
3. For good stability of the converter, any criteria need to be ensured?
thank you,
Johnson John
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi TI Team,
1. Can you please clarify difference between TPS563207 and TPS563207S ?
2. Is there any limitation on Max output capacitance?
3. For good stability of the converter, any criteria need to be ensured?
thank you,
Johnson John
Hi Johnson
1. Only one difference, 207S has higher Vref accuracy(1.5%) and 207 is 2%.
2. Recommend to use following the range in the table.
3. Good stability is judged differently by different customers. a method commonly used to evaluate stability, the Bode plot test, with a bandwidth less than 1/3 the operating frequency and a phase margin greater than 45°. thanks!