Part Number: LM2682
Hi all,
I am investigating using the LM2682 for a 3.3V--> -6.6V application. I attempting to test the device using the following circuit below, but I am receiving an output of -3.7V instead. If possible, could you verify that this setup is accurate? One thing of note is that I am using ceramic capacitors in this setup, so I am unsure whether this has an impact on device performance.

Thank you.