This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5176: Search right solution

Part Number: LM5176


hi Sir

I wan to design a PSU

Spec as below

Vin=24V

Vout=1V~48V

Io,max=10A

Po,max = 120W

the LM5176 is a best solution?

thanks

  • Hello Alex,
    Thanks for reaching out to us via e2e.

    Can you please describe more in detail what kind of device you are trying to build.
    When you say "PSU", are you thinking about a device like a lab supply / bench supply where you can set up a voltage and a current limit?
    Which kind of load(s) shall be connected?

    The LM5176 can NOT support a dynamically changeable current limit.
    The current limit is defined by the sense resistor (in the range of a few Milliohms).

    Please describe as detailed as possible.
    Thank you.

    Best regards
    Harry

  • Closed due to a duplicate thread.