This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV803: voltage supervisor on dual rail with TLV803 and opto coupler

Part Number: TLV803
Other Parts Discussed in Thread: TLV809, , TPS3711, , TPS3760, TPS3847

Hello,

I would like to supervise output from a dual rail DC DC converter.

It's a 24V to +-15V output.

Basically what I'm doing it's build a voltage divider that output 5V from +-15V. Then use the -15V as the GND reference of a voltage supervisor and the 5V voltage divider output as VCC input.
The Reset signal has to drive the LED of an optocoupler, and it does it straight without any pull-up. The optocoupler so drive an N-Channel and a P-Channel for the +15 and -15 loads.

I'm at present using TLV809, but because it's push-pull I've problem driving the led outputs, cause the divider does not works well with 75k and 15k, so I've to use 75ohm and 15ohm. Also it warms up due to the current that goes through it.

I'm wondering if the new TLV803 could work like the first image below, or I have to add an NPN like below.. or other?


Thanks!