Hi,
My customer is looking at using the TPS62442-Q1 for a dual output application but they are concerned about EMC. Can you provide more details about the phase shifted operation and how SS works with the phase shifting feature?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
My customer is looking at using the TPS62442-Q1 for a dual output application but they are concerned about EMC. Can you provide more details about the phase shifted operation and how SS works with the phase shifting feature?
Hi Tom,
Thanks for reaching out to us.
The dual internal buck converters in TPS6244x-Q1operate in the same switching frequency. However, the internal clock signal of converter 2 is phase shifted by 180 deg. C with converter 1. It means the converter 2 will only start switching at the midpoint of the switching cycle of converter 1. For example, the IC is set to operate at 2.2MHz. The converter 2 high-side FET will only turn-on after ~220ns delay with respect to converter 1. I hope the diagram below helps in showing the switching behavior of the two converters .
The spread spectrum clocking (SS) features also helps in reducing the converter's EMI emission by varying the switching frequency up to 20% above the nominal set by RCF. This helps in lowering input peak currents seen across the converter.
Please refer to the app note link below to have a better overview on the effects of operating two converters 180 deg. out of phase (page 8) and SSC function (page 14).
Best regards,
Excel
Hi Tom,
Just a gentle reminder. Do you still have queries?
Best regards,
Excel
Hi Tom,
Thanks for the confirmation.
I will close the thread now.
Best regards,
Excel