LM5177 Buck-Boost - In Use.xlsm
I have prototyped a 9V-50V input 20.5A 5.75A CC CV Battery Charging circuit and I am using this calculator...
However, the SLOPE resistor caused terrible inductor ring in my circuit, and with some trial and error, the 62k seemed to cause the least ringing...
The Comp network is an RC with a Capacitor in parallel, and after much trial and error, the most stable network seems to be with a 4.7k and 22nF RC with a 680pF in parallel...
However, around 15.5V-16V input, there is still a slight inductor ring...
This is not the main problem, but I believe it is related to the main problem...
The main problem is that anywhere in the boost or buck-boost range, the CC output will vary with the input voltage, from 0.6A at the worst (0.6A is at the same 15.5V - 16V Input) to 2.5A CC at the best...
Anywhere from 24V to 50V input, the output is a perfect 20.5V 5.7A CV CC....
Is my problem in the Comp network?