Other Parts Discussed in Thread: BQ24090
Attached to this posting is snippet from the BQ24316 data sheet pertaining to the undervoltage lock-out feature for the IN pin.
If lithium ion cell voltages are generally north of 3V and as high as 4.3V at end of charge, why is the designed-in UVLO level so low?
It seems to me that the UVLO threshold should have been, say, 4.7V to account for the highest possible cell voltage plus the voltage drop through the gating FET inside the BQ24316.
Because the IN pin serves a dual purpose (the input to UVLO/OVP functionality and the upstream side of the gating FET) it's not possible to externally force the UVLO threshold higher with a resistor divider. Plus any tinkering with the UVLO threshold would also move the OVP level higher, too.