This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5177: LM5177 to be a PSU(Power supply unit)

Part Number: LM5177
Other Parts Discussed in Thread: LM5176

hi Sir

we would like to design a PSU,spec as below, LM5177 is a suit soultion?

or LM5176

thanks

Vin=24V
Vout=1V~48V
Io,max=10A
Po,max = 120W

  • Hello Alex,
    Thanks for reaching out to us via e2e again.

    Same question, different device.
    What exactly do you mean when you say "PSU"?

    I can only ask you again to describe in more detail which application you are talking about / what exactly you want to build.
    Is it a bench supply for universal use with connectors where you can add any kind of load and with potentiometers for voltage and current setting?
    Please describe as detailed as possible.

    As long as you do not provide more information, we cannot really help you.
    Thank you.

    I am closing the other identical thread.

    Best regards
    Harry