Other Parts Discussed in Thread: BQ76952
Hi, we are currently designing a LifePo4 power bank and looking at BQ76942 might be suitable for our application. Can you recommend me a charging IC, fuel gauge and MCU that we can use in our product and if the BQ76942 is not overkill. We are looking for the most cost-effective ICs to be use in our product, so we do not select ICs with unwanted features.
Below is our requirement:
LifePo4 battery in 4S1P
Max charge current 10A
Stackable design (2 battery pack can be connected in parallel)
individual cell voltage, current, temperature, SoC, capacity remaining monitor in MCU through I2C
standard protection for battery like OVP,OCP etc.
Thank you in advance.