This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ28Z610-R1: Inquiries regarding BQ28Z610-R1 (fuel gauge)

Part Number: BQ28Z610-R1

Hi, TI experts

There is an inquiry from a customer regarding BQ28Z610-R1 (Fuel Gauge).

Currently, BQ24292IRGER (Charger IC) and 1-Cell (4.2V SDI Cell) are being applied.
The customer is planning to develop a configuration with two cells in a 1S2P arrangement using the BQ24292IRGER.

Q1)Currently using BQ28Z610-R1 (Fuel Gauge).
If we develop a new battery using the same method mentioned above, can we continue using the current BQ28Z610-R1 (Fuel Gauge)?

Please check. Thank you.

  • Hello,

    You can still use the BQ28z610-R1, but you will need to ensure you do not exceed the max capacity stated for this device.


    You will have to double all capacity data flash parameters (mAh) such as Design Capacity, Qmax, etc. 

    Regards,
    Jose Couso