Other Parts Discussed in Thread: LM2936
Hi,
I am comparing the use of LM2931 vs LM2936. Both are being used with a 15V input and a 5V output, well within range of both.
It was noticed that a series input resistance of 1.8k could be used on the 2936 (for protection), but not on the 2931. I am having trouble identifying the portion of the datasheets that shows where this is / is not allowed.
The 2936 has a lower Iq than the 2931, but considering that LDO is unloaded I did not expect the 2931 to be unable to maintain 5V (maintains 1.67V at 15V input).
When reducing the input resistance to half (900ohm) on the 2931, the LDO regulates slightly higher (2.2V). When removed completely it does achieve 5V regulation.
The output capacitance between these is different (10uF VS 100uF) and I did not change these between tests, could the 10uF allow regulation with no input resistance, but not allow it with such an input resistance?