This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UC1846: GENERATING COMPLEMENTARY PWMS without complete smps

Part Number: UC1846


Hello:

How do I generate stable 10 kHz to 1 MegHz complementary PWMs from UC1846 or any other suitable controller without making a complete SMPS solution?

On board, we just want to have 1 chip controller that generates 2 PWMs with deadtime.

Appreciate any help in the matter.

-r