Hi, I need help understanding various sections of the BQ25570 datasheet.
1) It is mentioned that the Minimum Input Voltage for Cold start was tested under the condition VBAT < VBAT_UV.
Would it be okay if my application initially has VBAT is greater than VBAT_UV? (When the battery is almost fully charged)
2) Why is sampling at 80%of input source voltage significant?
3) Regarding battery flags
If I understand it correctly, VBAT_OK_PROG flag will be set when VBAT decreases below VBAT_OK_HYST (max.) - 50mV right?
What function does this serve and why do we need two flags?
Sorry if there are too many questions, as I'm new to battery management and want to be sure.
Appreciate any help in understanding this. Thanks!