This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5180-Q1: Check the more detail information

Part Number: LM5180-Q1
  1. Is the limited duty 60%?(it always make the assumption that duty of IC is 60%  in datasheet)!?
  • Hi Chang-yi

    The max Duty is considered to be 70%. 

    Larger Duty usually means larger I_pk and I_rms for secondary, which means higher conduction loss and that the user will need to select a larger current rated diode.

    Thanks and best regards.