Part Number: LM5023
Hello.
My name is Eunseok,
I have a question while looking at the block diagram of LM5023.
I know you're busy, but could you answer a few questions?
1. In soft start operation, there are two n-channel mosfets inside, but isn't the mosfet that receives the EN signal as the gate signal a p-channel?

--> I understand that the EN signal is always HIGH, but if an N-channel MOSFET is used, the capacitor of the SS pin is not charged.
2. There is an N-channel MOSFET that receives the LEB signal of the CS pin as a gate signal. Is it a P-channel MOSFET?
If the N-channel MOSFET is correct, will the LEB signal be HIGH at the beginning of the LEB and then change to LOW after the LEB delay time?

3. What is the function of the tRESTART block that receives the output of the QR pin's Demagnetizing comparator as input?
Is it a simple delay role?

I have a lot of questions, so please understand.
Sincerely yours,
Eunseok