Part Number: BQ27531-G1
Other Parts Discussed in Thread: BQSTUDIO, BQ24192
Hi,
We use in our project the charger bq24192 together with the gasgauge bq27531. So we have NOT directly acces to the register of the charger. The bqstudio software communicate with the gasgauge bq27531 and it allows to change the settings for the gasgauge and charger.
But i'm wondering how to do this, for example i want to disable the watchdog timer, so I have to set in REG05, Bit5 and Bit4 to 0.When i acces the register through bqstudio it shows that the mentioned Bits are reserved, see the picture.

Has anybody an idea how to overcome this?
Regards,
Alex