This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS63000-Q1: When VIN is in the range of 1.8V to 2.2V, current limiting occurs.

Part Number: TPS63000-Q1

Hello
we are using TPS63000IDRCRQ1 in our project.
When VIN is in the range of 1.8V to 2.2V, a large current flows through the device independently, causing current limiting(The power supply unit will flow up to the limiter 800mA).
VCC5.3V=0mA (no load).
Please tell us the cause and the solution.
Thank you.

L1 3.3uH
C2 0.1u
C4 10u
C5 100p
C8 0.1u
C9 47uF
R5 100
R15 1.74M
R16 180k

-NG Waveform(VIN=1.8V)                                                     -OK Waveform(VIN=2.5V)