Hi,
I designed a costum board by takind an example of TPS2372-4EVM-006 and it works. I have a problem when ı set resistor values of CLSA and CLSB. I assigned CLSA pin as 63.4R and CLSB pin 90.9R for 70w power request from PoE switch (25w each port).
TPS2372-4 (or poe switch) isn't supposed to allow power (or handshake). I am always getting power 50v. (AMPS_CTL is disabled or not)
when I set CLSA pin as 63.4R, TPL indicator is always on even if I changed CLSB pin resistor value.
for CLSA pin as 90.9R, no indication is on. Changing the CLSB resistor value does not change the indication.
last one If I remove resistors, BT indication is on.
I don't want TPS2372-4 to handshake with the unsupported device.
Can you help to figure out the problem?
thank you
Ömer