Other Parts Discussed in Thread: BQSTUDIO
Hello,
I can't get out of the BQ40Z80 precharge mode and I can't start charging with the precharge current I set. I have added the bqstudio display and pre-charging settings.
Thanks,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
DSG FET is automatically activated when FET EN is used. I don't know why. 150823.gg.csv
Hello,
If you are turning on the PCHG and CHG FET manually via the toggle commands, please try using these commands with the FET_EN = 0.
Regards,
Anthony Baldino
Im not sure what your setup is, but if you don't have PCHG_COMM = 1 in the FET Options the BQ40Z80 will use the PCHG fet output as the precharge fet rather then the CHG fet and will wait for PACK to be equal to BAT.
If you do not have a dedicated precharge circuit attached to the PCHG pin, then you need to set PCHG_COMM = 1.
Be careful, this will result in high inrush current if you are charging a capacitive load.