Other Parts Discussed in Thread: LM337
I seek to have a very low noise dual rail supply (+-42.5V/50mA). The power rails will be generated by two isolated 48V to 42.5V DC/DC converters. To clean the positive side, I can simply use the TPS7A4001 as recommended to achieve the 42.5V/mA output. However, I cannot find equivalent performance and voltage rating with the negative LDO selection, but I read that I can connect the positive input of the negative supply to VIN, negative input of supply to GND, then connect the output of the LDO to GND to achieve the -42.5V regulation. I can do this as long as the negative supply is galvanically isolated. Will this work specifically with TPS7A4001? Anything I should watch out for?: