Other Parts Discussed in Thread: BQ76905,
I'm attempting to utilize the BQ25171-Q1. I intend to connect two 18650 lithium-ion batteries in series. Depending on the operational scenario, my design draws up to 1A from the battery, with a typical operating scenario being around 100mA. Is the BQ76905 BATTERY BALANCER necessary for my design? While I acknowledge that having it would be beneficial, I'm interested in understanding whether it is indispensable and the level of necessity.
Regards JH Park