Hello Support Team
On the TPS78433QWDRBRQ1 the EN is pin7 (pin6 is not connected) and on the B-Version TPS78433QBWDRBRQ1 the EN is pin6 (pin7 is not connected). The data sheet states that the respective unconnected pin should be connected to GND or floating. Can I create a single layout (pin6 and pin7) on IN, or should I better create two footprints?
Many thanks in advance
Beni