This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM27762: Unable to simulate the LM27762 in WEBENCH

Part Number: LM27762

I'm using the LM27762 to generate +5 and -5 voltages and I would like to use WEBENCH to simulate performance with various capacitors and resistors, as mentioned on page 13 of the datasheet.   When I choose LM27762 in WEBENCH (webench.ti.com/.../switching-regulator)  it says "Sorry, we could not find LM27762".  I also can't get it to find the part when I enter my input and output voltages.  I would like to see the switching waveforms at my expected current load.

In the meantime, I'm trying to reduce the output resistance on the -5v output because I'm only achieving -4.6v at my load of 60mA. What is the value of Rsw to use in Equation 2? With no load current the voltage measures -5v, so I know the feedback resistors are correct.

My input voltage is 5.5v and I'm using these components:

R1 237k

R2 75k

R3 255k

R4 82.5k

C1 0.1uF (flying capacitor)

Cp. 4.7uF