On my PCB, the BQ24295 is not giving voltage on Vsys, the Vsys only has voltage when i connect the battery, and after i disconnect the battery the system oscilates and the MCU resets it self because of low voltage.
This is the schematic:
I realize that i didn´t apply the TS resistor divider (naively i didn´t add it because i thought that if i wasn´t going to use the thermistor then i wouldn´t need the resistor divider). I tryed adding the resistor divider externaly but it didn´t work either (i used a 10k/10k resistor divider and also tryed with a 5k1/10k resistor divider). I did realize though that:
Without the resistor divider on the TS pin i had a "hot thermistor fault", and everything else seems to be ok (SYS status reg gave me 10 00 1 1 0 0), but the fault reg gave the NTC_FAULT to 1.
With the resistor divider i got not faults on the register, but the system register marked 00101100, so it seems like it doesn´t detect the input voltage now.
I need that the circuitry works with and without the battery on boot, what i´m doing wrong?
thanks!!